- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Associate an unassigned axis to a motion group
If an axis is created and unassigned to a motion group, it is unavailable for use. Use the
Axis Assignment
tab in the Motion Group Properties
dialog box to assign and remove an axis to and from a motion group.To associate an unassigned axis to a motion group:
- In the Controller Organizer, right-click the motion group and clickProperties.TheAxis Assignmenttab lists the axes that areAssignedandUnassignedto the motion group.
- Select the axis from theUnassignedlist and selectAddto add the axis to the motion group.
- To remove an axis from the motion group, select the axis from theAssignedlist and selectRemove.
- SelectOK.
Provide Feedback