HMI input labels for PBL
Use the
HMI - Input label
tab on the PBL Properties
dialog box to add labels that appear on the inputs on the HMI.To enter HMI input labels for Process Boolean Logic (PBL) instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
.
- In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Under theHMItab, selectInput label.
- In theInput labelbox for each input, enter a label that appears on each input on the HMI.
- When online with the controller, monitor theDevice stateandDevice issuesindicators at the bottom left of the dialog box:
- Device state. Displays the current device state depending on the value of the Out_Live parameter. Use theHMItab to enter text in theText to display when output equals 0andText to display when output equals 1boxes.
- Device issues. Displays fault conditions:None, orConfiguration error.
- SelectApply.
Provide Feedback