Print spooler error. Unable to start print job.

The print spooler was unable to print to the requested report. The error message you receive indicates one of the following conditions:
Insufficient memory
You may need to close other applications to free more memory, or you may need to add additional RAM memory to your computer.
An invalid printer/port was specified
Make sure that your printer is properly configured.
If you specified the Generic/Text Only option, make sure that you have entered a valid output file name.
An invalid print range was specified
Make sure the print range you specified is not greater than the number of rungs/lines/sheets in your routine, and that you have not specified a negative number.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.