ServoFault

Applies to: Servo axes.
ServoFault is a 32-bit attribute. Its value is set upon the occurrence of any of the following faults. Click a fault in the following list for information about that fault.
Bit #
Fault Name
0
1
2
3
4
5
6
7
8
9
10 - 31
Reserved
The occurrence of a ServoFault sets the PhysicalAxisFault attribute and bit #0 of the AxisFault attribute.
To clear a ServoFault, you must diagnose and clear the underlying fault. The following instructions can be used to clear both the underlying fault and the ServoFault:
  • Fault Reset (MAFR) instruction, to clear all motion faults for an axis.
  • In the case of a shutdown, a Shutdown Reset (MASR) instruction, to return to an axis ready operating state.
  • For a grouped axis: Motion Group Shutdown Reset (MGSR) instruction, to transition a group of axes from the shutdown operating state to the axis ready operating state.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.