Addressing the Workforce Skill Shortage
The path to digital transformation in manufacturing contains multiple hurdles, among which the workforce skill shortage stands out. The rapid integration of new technologies necessitates a workforce that not only understands these technologies but also knows how to leverage them effectively. However, the lack of tech-savvy talent is a pressing issue that has proven to be a major roadblock in many manufacturing companies' digital transformation journeys.
As we approach a decade where numerous ‘baby boomers’ are set to retire, a looming uncertainty persists regarding their replacements. The question of who possesses the necessary skills and expertise to fill these soon-to-be vacant positions is a significant concern. The standard practice involves hiring and seeking talent, but the transition of newly onboarded talent to the same level of proficiency as the retiring worker is often a lengthy process.
Fortunately, emerging techniques and methodologies can expedite this process, ensuring new talent becomes skilled and expertly versed in their roles in a short period. The popular notion that proficiency in a role requires 10,000 hours of practice can be mitigated through strategic upskilling techniques. Such techniques not only address workforce shortages but also reduce the time required for workers to reach peak productivity.
It is evident, based on the 750,000 manufacturing jobs currently unfilled in the US alone, that organizations are experiencing a workforce shortage. Still, as new talent enters the workforce and adopts technologies designed to expedite their productivity, the total cost of ownership (TCO) and return on investment (ROI) become justifiable. The technology's business case is valid from day one, as it shortens the period from the time the worker joins until they are productive.
Furthermore, these technologies are versatile and can be applied in other areas, such as reducing inspection time and increasing operational effectiveness. This presents an additional benefit, further reinforcing the need for companies to adopt new technologies to navigate the challenges of the impending workforce shortage.