Uninformed users won’t know how much safe gas is entering the enclosure, which means they won’t know the proper volume exchange. A flow measurement is required to determine the necessary time that must pass for a successful purging. Some purging systems will measure the flow for determining purge time.
4. Failure to Address Combustible Dust
Another common and dangerous mistake is not recognizing that dust being produced in the plant is combustible. A raw material used during the manufacturing process might not be listed as combustible, but dust formed during the process itself could be combustible.
Additional testing is normally required for full and complete certification, including heat measurements from the equipment for T-codes, overpressure testing of the enclosure to help ensure it doesn’t break or permanently deform, and flow checks to confirm all points within the enclosure are purged and pressurized properly.
Other standards and requirements might apply to other parts of the system, including wiring, terminations, gas handling elements and alarm management. By using certified purge and pressurization components, the implementation and final certification of the system will be easier, faster, and hopefully less expensive.
Although the area classification is important in identifying the type of purge system required for the application, the above issues apply to both NFPA 496 Type Y, Z, X (North American requirements), and EN/IEC 60079-2, Type pyb, pxb, pzc (European and International requirements) and local codes.
An understanding of the applicable standards and the hazardous area classification is important in applying any hazardous area protection method. Safety is the ultimate goal and should always be the first consideration in operating equipment in hazardous areas.
Pepperl+Fuchs, Inc., based in Twinsburg, Ohio, is participating Encompass™ Product Partner in the Rockwell Automation PartnerNetwork™ program. The company develops and manufactures hazardous location protection products and components for electronics used in the global process automation market.
The Journal From Rockwell Automation and Our PartnerNetwork™ is published by Putman Media, Inc.