Task properties
This table describes task elements.
Element | Description |
Description | Information that describes the program. |
Period | f the task is a periodic task, specify how often to run the task (1.000...2,000,000.000 µs). |
Priority | Specify the priority of a periodic task (1...15) |
Watchdog | Type the watchdog timeout for the task (1.000...2,000,000.000 µs) |
Trigger | Only used for event tasks. Specify the trigger for the event task. Type Axis Home, Axis Watch, Axis Registration 1, Axis Registration 2, Motion Group Execution, EVENT Instruction Only, Module Input Data State Change, Consumed Tag, or Windows Event. In L5X, this attribute is on the element. |
executeTaskNoEvent | |
disableAutomaticOutput | Type 1 (or true) to disable updates to outputs while the task executes. Otherwise type 0 (or false). The default for a periodic or continuous task is 0. The default for an event task is 1. |
inhibited | Type 1 (or true) to inhibit the task. Otherwise enter 0 (or false). |
Provide Feedback