Explorer bar
The explorer bar appears in the Explorer pane of the open project. Use the icons on the explorer bar to open the various explorers:
Item | Description |
---|---|
System . Open the System explorer. Use the System explorer to create FactoryTalk Smart Objects and the programs within the System Objects. | |
Devices . Open the Devices explorer.Devices explorer to view and manage the hardware used in the project. | |
Execution . The Execution explorer contains the executable logic of a project. Use the Execution explorer to create a controller application and to view and change tasks, programs, and routines. | |
Library . Open the Library explorer. Use the Library explorer to add new definitions of Add-On Instructions and FactoryTalk Smart Objects and to add new Data Types to the project. |
Provide Feedback