Export an MCC lineup

Export an MCC lineup to use the lineup in the Logix Designer application.
To export an MCC lineup:
  1. Open or create a project.
  2. Select
    File > Export MCC lineup
    to open the
    Export MCC Lineup
    dialog box.
  3. Select
    Export
    to add the MCC lineup to a zip file. When the lineup has zipped successfully, the
    Export MCC Lineup
    dialog box opens.
  4. Select
    Download
    to download the zipped dataset to the computer's
    Downloads
    folder.
  5. Download the
    update_dataset
    file.
  6. Copy the file to the original dataset folder.
  7. Run
    Update_dataset.exe
    as an admin.
  8. If this is the first time you are installing the dataset on your computer, leave the
    Destination folder of Database files
    as the default. If the lineup is already installed on your computer, select a new location for the database and documentation.
  9. Restart your computer and open the IntelliCENTER software version six to access the dataset containing the changes you made in FactoryTalk Design Studio.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.