Greater Than or Equal To (GE)
When enabled, the Greater Than or Equal To (GE) instruction tests whether Source A is greater than or equal to Source B.
![RSL5K_GEQ String Compare Flow Chart](/content/dam/dita/en/factorytalk-design-studio/current/online-help/topics/graphics/rsl5k_geqstringcompareflowchart.png/_jcr_content/renditions/original)
![GE ladder example](/content/dam/dita/en/factorytalk-design-studio/current/online-help/topics/graphics/ladder_GE_example.png/_jcr_content/renditions/original)
Available Languages
Ladder Diagram
![GE ladder instruction](/content/dam/dita/en/factorytalk-design-studio/current/online-help/topics/graphics/ladder_GE.png/_jcr_content/renditions/original)
Operands
There are data conversion rules for mixing numeric data types within an instruction. See Data conversions.
Ladder Diagram
Numeric Comparison
Operand | Data Type | Format | Description |
---|---|---|---|
Source A | SINT INT DINT LINT USINT UINT UDINT ULINT REAL LREAL | immediate tag | Value to test against Source B |
Source B | SINT INT DINT LINT USINT UINT UDINT ULINT REAL LREAL | immediate
tag | Value to test against Source A |
String Comparison
Operand | Data Type | Format | Description |
---|---|---|---|
Source A | String type | immediate literal value tag | String to test against Source B |
Source B | String type | immediate literal value tag | String to test against Source A |
Affects Math Status Flags
No
Major/Minor Faults
See
GE String Compare Flow Chart
for faults. See Index through arrays for array-indexing faults.
Execution
Ladder Diagram
Condition/State | Action Taken |
---|---|
Prescan | N/A |
Rung-condition-in is false | Set Rung-condition-out to Rung-condition-in |
Rung-condition-in is true | Numeric compare: If Source A and Source B are not NANs and Source A is greater than or equal to Source B. Set Rung-condition-out to true else Clear Rung-condition-out to false. |
String compare: See GE String Compare Flow Chart. If output is false Clear Rung-condition-out to false else Set Rung-condition-out to true | |
Postscan | N/A |
GE String Compare Flow Chart
![RSL5K_GEQ String Compare Flow Chart](/content/dam/dita/en/factorytalk-design-studio/current/online-help/topics/graphics/rsl5k_geqstringcompareflowchart.png/_jcr_content/renditions/original)
Example
Ladder Diagram
![GE ladder example](/content/dam/dita/en/factorytalk-design-studio/current/online-help/topics/graphics/ladder_GE_example.png/_jcr_content/renditions/original)
Provide Feedback