Display an object to a user group

Make a graphical object accessible only for specific users.
Prerequisites
Add a graphical object that you would like to show only to a specific group of users. See Create a graphic object from a type.
For example, create an
AdminPane
object that is only visible to the Admin group members.
  1. To display an object to a user group
  2. In the pane, select the graphical object.
    For example, select
    AdminPane
    .
  3. In the pane, create a dynamic link between the
    Visible
    property and
    Aliases
    {Session}
    Session
    Groups
    TargetGroup
    .
    TargetGroup
    The group of users that you want to make the graphical element visible for. For example,
    Admins
    .
    For more information about dynamic links, see Create dynamic links.
The
Visibility
property of a graphical object has a Boolean value. If the current user at runtime is a part of the selected group, the value of the property at runtime is set to
True
and the object is visible in the UI.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.