Edit Project Properties
Project properties contain the name of the project and its description as well as a file history of your project from the time you uploaded it to FactoryTalk Design Hub. You can add notes to different versions of the project to track activity over time. You can also change which version of the project is primary (active) in the vault from project settings.
- From the vault, select the project. ThePropertiespane is displayed on the right side of the vault window.
- The properties panel sidebar opens with two tabs,PropertiesandHistory.
- InProperties, you can change the name and description of the project by clicking on theEditpencil next to the item.
- InFile history, you can see the history of changes to the project since it was originally uploaded.
- SelectADD NEW FILEto add another version of the project file to the history.
- Select theAddicon next to the project to add a note to a version of the project.
- Select the note icon next to the project to edit the note.
- Select the option button to make that version of the project the primary version in the vault.
- SelectSaveto apply the changes.NOTE: TheSAVEbutton is enabled if there are unsaved changes. If you close the panel without saving the changes are discarded
Provide Feedback