Attribute and Parameter Org
In the
Logix Designer
application, the motion axis parameters and attributes are organized by functional group. You will only be presented with the attributes or parameters that are applicable to the category you choose and the configuration values you input.For example, when you choose Planner, only the attributes or parameters that relate to the Planner Group appear.
Drive parameters are also available from the organizer.
Provide Feedback