Axis Test Mode Config Attributes

These attributes are the configuration-related attributes associated with a Motion Control Axis.
Axis Test Mode Configuration
Usage
Access
Data Type
Default
Min
Max
Semantics of Values
Required
Set/GSV
USINT
-
-
-
Enumeration:
0 = Controller Loop Back
1-255 = Reserved
The Axis Test Mode Configuration attribute allows the selection of the desired test mode model that determines how the axis simulation is performed. Currently, only the Controller Loopback model is supported.
Axis Test Mode Enable
Usage
Access
Data Type
Default
Min
Max
Semantics of Values
Required
Set/GSV
USINT
-
-
-
Enumeration:
0 = Disabled
1 = Enabled
2-255 = Reserved
The Axis Test Mode Enable attribute allows the enabling or disabling of the Axis Test Mode on a certain axis.
Cyclic Read Update List
Axis Test Mode
Axes with the Test Mode attribute set to Enabled and that are configured for Controller Loop Back simulate Axis Safety Data A and B attributes.
Attribute Name
Axis Test Mode Support
(Test Mode Configuration)
Safety Data A
Controller Loop Back: v36
Safety Data B
Controller Loop Back: v36
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.