Configuration Fault Attributes
These are the configuration fault related attributes associated with a Motion Control Axis.
Attribute Error Code
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - All | Get/GSV | T | INT | - | - | - | Refer to CIP Error Codes |
CIP Volume 1, General Status Code returned by the erred set list service to the module.
Attribute Error ID
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
---|---|---|---|---|---|---|---|
Required - All | Get/GSV | T | INT | - | - | - |
Attribute ID associated with non-zero Attribute Error Code.
Provide Feedback