Saving ACD File vs Upload of Project
The following is an example of a sequence of events that can generate an APR fault.
- Make an online change to an axis attribute that generates an APR fault.
- Rehome the axis.This is normally done so APR will restore axes positions after a download.
- Save your project.
- Download your project.
An APR fault occurs because saving the project only uploads the tags, not the changed attributes.
NOTE:
Upload the project to save the changed attributes and prevent an APR fault on a subsequent download.
Provide Feedback