Start Inhibits Attributes

These are the Start Inhibit related attributes associated with a Motion Control Axis Object instance. Start Inhibits are conditions that prevent transition of the axis from the Stopped State into any of the operational states.
CIP Start Inhibits
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Required - All
Get/GSV
T
WORD
-
-
-
Enumeration:
0 = Reserved
1 = Axis Enable Input
2 = Motor Not Configured
3 = Feedback Not Configured
4 = Commutation Not Configured
5 = Safe Torque Off Active
6 = Converter Bus Unload
7 - 15 = Reserved
A bit map that specifies the current state of all standard conditions that inhibits starting of the axis.
Axis Test Mode
Axes with the Test Mode attribute set to Enabled and that are configured for Controller Loop Back simulate these enumerated values for the CIP Start Inhibit attribute.
Enumeration
Axis Test Mode
(Test Mode Configuration)
5 = Safe Torque Off Active
Controller Loop Back: V36
CIP Start Inhibits - RA
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Required - All
Get/GSV
T
WORD
-
-
-
Enumeration:
0 = Reserved
1 = Volts Hertz Curve Definition
2 = Motor Feedback Required
3 = Speed Limit Configuration
4 = Torque Prove Configuration
5 = Safe Torque Off
6 = Safety Reset Required
7 = Safety Not Configured
8 = Stop Command Active
9 = Feedback Device Reset
10 = Brake Malfunction
11 = AC Line Contactor Input
12 - 15 = Reserved
A bit map that specifies the current state of all
Rockwell Automation
specific conditions that inhibits starting of the axis.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.