Text Chart

Text Chart

Perform the following steps to create Text Chart:
NOTE:
Chart settings like Configuration, Style and Sorting & Ranking are not available for Text charts.
  1. Open a Storyboard, hover the mouse on a chart tile and click the [] icon to maximize the tile.
  2. Click the [] icon. The Chart Settings window displays.
    Attribute
    Under the Type tab, the list of available chart type displays.
  3. Click [Text Chart]. The "Configuration, Style and Sorting & Ranking are not available for Text charts." information dialog displays.
    Chart Settings
  4. Click [Apply].
  5. The text box displays, enter the desired text, and click [Apply].
    Text Chart
    The Text chart displays.
    Chart Settings
  6. Click [Edit] to edit and format the text in the chart.
    Storyboard Updated
  7. Click the [] icon to import image or click the [] icon to insert a link to the chart.
    Storyboard Updated
  8. Click the [] icon to minimize the chart. The updated Storyboard displays.
    Storyboard Updated
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal