Add a controller
Add a controller to a project to connect the controller with the project. Add controllers from the
Devices
explorer. - On the explorer bar, selectDevices.
- InDevicesexplorer, selectHamburger Menu, then selectNew device. TheAdd device to projectdialog opens.
- In theAdd devices to projectdialog, underCategory filter, selectController.
- Select a controller from the list and then selectContinue.
- UnderPending to configure, enter the controller information and then selectFinishto add the controller to the device list.TIP: Controller names:
- Can contain up to 40 valid characters.
- Can contain only alphanumeric characters and underscores.
- Must begin with a letter or underscore.
- Cannot include consecutive underscores.
- Cannot end with an underscore.
TIP: Additional options to add a controller from either the:- Device list, at the top of theDevice list, selectAdd device.
- Executionexplorer
. Select
Hamburger Menu, and then selectAdd controller. In theAdd controllers to projectdialog, select a controller from the catalog list.
Provide Feedback