- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Develop a label with a localized engineering unit
Create a simple interface that displays temperature in a format that is adjusted for a logged in user locale.
Application example - Celsius degrees (it-IT)

Application example - Fahrenheit degrees (en-US)

NOTE:
Download a sample project:
LocalizedEngineeringUnitLabel.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Application design example

In
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
FactoryTalk Optix Studio
, select 
Run
Provide Feedback