Scroll view example
Use this object to provide a panel that includes scroll bars, so that it can contain content larger than the panel itself.
TIP:
Scroll view
supports:
- Touch and multitouch gestures, such as pan or pinch-to-zoom.
- Keyboard and mouse operation, such as thecombination to zoom-in or zoom-out.
Scroll view example

Use case
Display overview information, drawings, or other items that are larger than the main application container.
Provide Feedback