Objects

Objects

An object is an element that identifies a physical object such as a motor or a non-physical object such as a digital alarm.

Object components

An object can contain:
  • Display name
  • Description
  • Variables
  • Nested objects

Object example

A physical motor is a mechanical object with specific operational characteristics such as acceleration, speed, and torque. The
Motor
object in the project is an object that contains the same properties.
Motor object properties
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal