Add an instance of a graphic object

Add an instance of a graphic object

Add a graphic element to the User Interface Editor to create an instance of the graphic element and have the object or element appear in the
FactoryTalk Optix Application
at runtime.
  1. From
    Project view
    , double-click the window to which to add the graphic object. The User Interface Editor opens.
  2. From
    Type view
    , select the desired folders to navigate to the graphic element and then and drag the graphic object to the window.
An instance of the graphic object is added to the window and
Project view
. If you add more instances of the same graphic object to the same window, the object name is appended with an increment number in both
Project view
and the
Name
property.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal