Create a local library

Create a local library

Create a custom local library to store templates of objects and variables.
TIP: To use a custom local library on another computer, copy the folder with the library name from
C:\Users\
UserName
\Documents\Rockwell Automation\FactoryTalk Optix\Libraries
to the same location on another computer. Alternatively, you can use remote libraries. See Create a remote library.
  1. From the main toolbar, select
    Template Libraries
    Template Libraries
    .
  2. In
    Template Libraries
    , select
    Add
    Add
    and select
    New library
    .
  3. (optional) Enter a name for the library.
New library appears in
Template Libraries
.
Add templates to your library. See Create a template from an object or variable.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal