Variables

Variables

A variable is an attribute of an object. Assign a value to a variable to display the value at runtime.
View variables in
FactoryTalk Optix Studio
from either:
  • Project
    view
    . Navigate to the folder containing the variables. The
    UI
    folder cannot contain variables.
  • Properties
    . Select an object, type, or variable in
    Project
    view
    or select and object in the editor. The variables or properties for the selected item appear in
    Properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal