- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Import nodes at runtime
Importing nodes at runtime requires an initial configuration.
- InProject view, select anOPCUAClientobject.
- InProperties, select
.A list of nodes appears underRuntime configurations. - UnderRuntimeConfiguration:#
- SetLocal destination node.
- SetRemote source node.
- InContent synchronization mode, select an option.NOTE: Import graphic and LocalizationDictionary objects in theImport onlymode.
- InInclude remote source nodes, select either:
- Trueto import the source node and child nodes.
- Falseto import only the child nodes.
- To enable the events generated by the selected nodes:
- SetEnable event synchronizationtoTrue.
- InEvent type, select
and inside , select the event type.
Provide Feedback