Backup a project
FactoryTalk Optix Studio
automatically creates backups of projects. Projects are automatically backed up:
- When you save a project
- When you update a project to make the project compatible with a more recent version ofFactoryTalk Optix Studio
- Every time you update a project to repair a corrupted project. See Restore a project.
The default location for the backup folder is:
%localappdata%\Rockwell Automation\FactoryTalk Optix\Studio\Backups\[Project Name]
Each of the project folders consists of other subfolders with these different types of backups:
- Automatic: three backups, performed when saving the project
- Recovery: one backup, performed when a corrupt project is opened and repair attempted inFactoryTalk Optix Studio. See Restore a project.
- Upgrade: two backups, performed when updating the project to make it compatible with a newer version ofFactoryTalk Optix Studio.
Provide Feedback