- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Configure a recipe schema
You can configure a recipe schema by using a dedicated interface built into
FactoryTalk Optix Studio
.
TIP:
You can also add a recipe manually. See Configure a recipe schema manually.
- From theFactoryTalk Optix Studiotoolbar, select
Open dashboard page. - In the central pane, selectI want to configure a recipe.
- Select an existing recipe or create a new recipe:
- To create a new recipe:
- SelectNew recipe.
- EditName.
- Complete theTarget node.
- SelectNext.
- To edit an existing recipe:
- Select an existing recipe.
- Edit the recipe properties.
- To duplicate an existing recipe:TIP: Duplicating an existing recipe enables you to quickly create a new recipe based on the existing recipe.
- Right-click an available recipe and selectDuplicate.
- If needed, edit the recipe properties.
- SelectNext.
- Select an existing database or configure a new database:
- To use an existing database:
- Select an existing database.
- If needed, edit the database properties.
- SelectNext.
- To create a new database:
- SelectNew database.
- If needed, edit theNameandTypefields.
- SelectNext.
- If needed, edit the database properties.
- SelectNext.
- To duplicate an available database:TIP: Duplicating an existing database enables you to quickly create a new database based on the existing database.
- Right-click an available database and selectDuplicate.
- If needed, edit the database properties.
- SelectNext.
- Select the recipe parameters to use.TIP: You can show or hide variables (parameters) nested in other variables by using theNested variablestoggle. You can quickly find the parameters that you want to select by using theSearchfield.
- SelectNext.
- Review the settings.
- SelectExit.
Provide Feedback