- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Duplicate a recipe schema
Duplicate a recipe schema based on the existing recipe schema.
- From theFactoryTalk Optix Studiotoolbar, select
Open dashboard page. - In the central pane, selectI want to configure a recipe.
- Right-click the available recipe schema and selectDuplicate.
If necessary, edit the duplicated recipe schema. See Edit a recipe schema.
Provide Feedback