Create the System object

Create the System object

The System object allows users to view and configure certain system settings, such as those that provide the date, time, time, and IP addresses of network interfaces and allows the user to restart the system at runtime.
Create one
System
object per project.
  • In
    Project view
    , right-click
    Model
    and then select
    New
    All
    System
    System
    .
    System1
    appears in
    Project view
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal