- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Zoom in and zoom out a trend chart
You can zoom in and zoom out a trend chart in three different ways.
- Use the pinch-to-zoom gesture.
- Place the mouse pointer in the area of interest and scroll forward or backward with the mouse wheel.
- Select the Trend graph and select+or-.
Provide Feedback