Pull preview

Pull preview

Pull changes from the remote repository to see conflicts between the local project and the remote project.
The preview shows changed values and removed objects. Keep either the change in the local project or the change in the remote project. An example
Pull preview
may include:
Item
Description
A
Rows of highlighted conflicts or changes.
B
Select
Take all local
to accept all of the local changes. Select
Take all remote
to accept all of the changes in the remote repository.
C
Filter the changes in the preview by displaying
All
project content, only
Updates
to the project, or only
Conflicts
in the project.
D
Select   to navigate to and expand the next conflict, or select navigate to the previous conflict.
Select a conflict to the left in a row to accept the local change. indicates local content. Changes in values are indicated and removed objects are crossed out.
F
Select a conflict to the right in a row to accept the remote change. . indicates remote content. Changes in values are indicated and removed objects are crossed out.
G
An icon in a row indicates:
  •   A conflict exists between the local and remote project.
  • A conflict was resolved by selecting either the local or remote change in the row.
  • A change exists in the local or remote project.
  • An object was added.
  • An object was removed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal