Compare versions of a project

Compare versions of a project

Compare two different versions of a project by selecting two different committed changes in
View history
.
  1. In the open project, select
    View History
    .
  2. In
    View history
    , select in two different commits to compare.
    TIP: The differences between the commits are highlighted.
  3. (optional) To toggle the content that appears in
    View history
    , select either:
    • All
      . Toggle to show all content in the project.
    • Updates
      . Toggle to show only the differences between the selected commits. This is the default.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal