- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- OPC UA tutorial
- NetLogic tutorial
- Object and variable references
Editable label
Display an editable text.
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Text | Text | Text to display and possibly changed by the user. | |
Text horizontal alignment | TextHorizontalAlignment | Indicates where the text is positioned on the horizontal axis. | |
Text vertical alignment | TextVerticalAlignment | Indicates where the text is positioned on the vertical axis. | |
Word wrap | WordWrap | Enable/disable the automatic word wrapping when the text is wider than the container. Ignored when the object width is automatic or when text abbreviation is set. | |
Text trimming | Elide | Text trimming mode. Insert three dots (...) in the indicated position when the text is too long for the available space. Ignored when the object width is automatic or when word wrap is set. | |
Font family | FontFamily | Font family. | |
Font weight | FontWeight | Font weight. | |
Font italic | FontItalic | Enables/disables italics in the text. | |
Font size | FontSize | Font size. | |
Text color | TextColor | Color of the text to display. | |
Border color | BorderColor | Color of the polygon border. | |
Editable | Editable | Enable/disable the change of the value directly in the chart. | |
Visible | Visible | (Inherited from Element) | |
Enabled | Enabled | (Inherited from Element) | |
Opacity | Opacity | (Inherited from Element) | |
Left margin | LeftMargin | (Inherited from Element) | |
Top margin | TopMargin | (Inherited from Element) | |
Right margin | RightMargin | (Inherited from Element) | |
Bottom margin | BottomMargin | (Inherited from Element) | |
Width | Width | (Inherited from Element) | |
Height | Height | (Inherited from Element) | |
Horizontal alignment | HorizontalAlignment | (Inherited from Element) | |
Vertical alignment | VerticalAlignment | (Inherited from Element) | |
Rotation | Rotation | (Inherited from Element) |
Events
Modified text
- BrowseName
Provide Feedback