- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Set margins
Edit the space around an object.
Prerequisites
- To edit object margins
- InProject view, select the object to edit.
- InMarginproperties, enter the value for the space between the edge of the parent object that contains the object.
margin
Provide Feedback