- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Spin box
Increases or decreases a numerical value by entering the value or using buttons.
Use case
Change the value of an analog variable, such as a temperature setpoint.
Example

Provide Feedback