- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Data controls
Use data controls objects to visualize data in your application interface. Get data from project nodes or a database.
Object | Description |
---|---|
Select items from a drop-down list at runtime. | |
Select items from a list box at runtime. | |
Display data in a table. | |
Display trends that present values from one or more variables that are logged or read in real time. | |
Display the value of two-dimensional variables in a graph. | |
Display data in the form of a pie chart. | |
Display data in the form of a bar diagram. |
Provide Feedback