Draw an oval or circle

Draw an oval or circle

Use the
Ellipse
tool to draw and oval or circle.
  1. In
    Project view
    , double-click the container to include the object.
  2. In the editor toolbar, select
    Ellipse
    .
  3. In the editor, position the crosshair where the oval or circle is to begin.
  4. Drag to draw the oval or circle.
The object appears in the editor and in
Project view
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal