- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Create a style sheet
Each project you create from a standard template includes a style sheet. You can create additional style sheets for the project.
TIP:
Instead of creating your own style sheet from scratch, you can add a predefined style sheet. See Add a predefined style sheet. For example, you can add a dark style sheet.
- InProject view, right-clickUIand select .StyleSheetappears in#Project view.
- (optional) Hover-overStyleSheet, select#, and enter a new name for the style sheet.
style sheet
Provide Feedback