- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Users, groups, and roles
Users, groups, and roles are part of a security policy and determine how user access is controlled for an application at runtime. Add and manage users and groups from the dashboard page or
Project view
.Verify that certain screens or content is visible or enabled for only certain user groups or roles. Specify access by binding the property of a screen or graphic object to a Session variable.
To manage users, groups, and roles:
access
Provide Feedback