Create a motor values widget instance

Create a motor values widget instance

Create a motor values widget instance from the motor values widget type.
  1. In
    Project view
    , right-click
    MainWindow (type)
    and select
    New
    MotorValuesWidget
    .
  2. In
    Properties
    , create a dynamic link between
    Motor
    and
    ProjectName
    UI
    MainWindow (type)
    MotorListBox
    Selected item (Pointer)
    .
    For more information about dynamic links, see Create dynamic links.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.