- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Create the application interface
Create a button and a label that will change its text when you press the button.
- InProject view, expandUI.
- Right-clickMainWindow (type)and select .
- InProperties, setTexttoRun Script.
- InProject view, right-clickMainWindow (type)and select .
- InProperties, setTexttoOriginal label text.
- Arrange the interface elements.

Provide Feedback