- Getting started
- Creating projects
- OPC UA
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- NetLogic
- Tutorials
- Dynamic links tutorial
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Add objects
Add a label and either a ClockLogic NetLogic or a System object as the source of current time and date.
- Add a label to display the date and time:
- InProject view, right-clickMainWindow (type)and select .
- Hover-over the label, selectand enterDateTimeLabel
- Either:
- Import the ClockLogic NetLogic. See Import ClockLogic.
- Add and configure a System object. See System object.
Provide Feedback