Insert String (INSERT)

Insert String (INSERT)

This information applies to the
CompactLogix
5370,
ControlLogix
5570,
Compact GuardLogix
5370,
GuardLogix
5570,
Compact GuardLogix
5380,
CompactLogix
5380,
CompactLogix
5480,
ControlLogix
5580, and
GuardLogix
5580 controllers.
Use the INSERT instruction to add ASCII characters to a specified location within a string.
Available Languages
Ladder Diagram
Function Block
Structured Text
INSERT (SourceA,SourceB,Start,Dest);
Operands
There are data conversion rules for mixed data types within an instruction. See Data conversions. The INSERT instruction uses the following operands.
Ladder Diagram and Structured Text
Operand
Type
Format
Description
Notes
Source A
String type
Tag
String to add the characters to
String types are default STRING data types or any new string types you create
Source B
String type
Tag
String containing the characters to add
Start
SINT
DINT
Immediate tag
Position in Source A to add the characters
Enter a number between 1 and the DATA size of the Source.
Destination
String type
Tag
String to store the result
See Structured Text Syntax for more information on the syntax of expressions within structured text.
Description
The INSERT instruction adds the characters in Source B to a designated position within Source A and places the result in the Destination.
  • Start defines where in Source A that Source B is added.
  • Unless Source A and the Destination are the same tag, Source A remains unchanged.
Affects Math Status Flags
No
Major/Minor Faults
Type
Code
Cause
Recovery Method
4
51
The LEN value of the string tag is greater than the DATA size of the string tag.
  1. Check that no instruction is writing to the LEN member of the string type tag.
  2. In the LEN value, enter the number of characters that the string contains.
4
56
The Start or Quantity value is invalid.
Check that the Start value is between 1 and the DATA size of the Source.
Execution
Ladder Diagram
Condition
Ladder Diagram Action
Prescan
The rung-condition-out is set to false.
Rung-condition-in is false
The rung-condition-out is set to false.
Rung-condition-in is true
The instruction executes.
The rung-condition-out is set to true.
Postscan
The rung-condition-out is set to false.
Execution
Structured Text
Condition
Action
Prescan
See Prescan in the Ladder Diagram table
Normal execution
See rung-condition-in is true in the Ladder Diagram table.
Postscan
See Postscan in the Ladder Diagram table
Example
When
temp_high
is set, the INSERT instruction adds the characters in
string_2
to position 2 within
string_1
and places the result in
string_3
.
Ladder Diagram
Structured Text
IF temp_high THEN
INSERT(string_1,string_2,2,string_3);
temp_high := 0;
END_IF;
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal