Replicated Attributes
These are the controller attributes that are replicated in the motion module.
- Acceleration Feedback
- Acceleration Feedforward Command
- Acceleration Feedforward Gain
- Acceleration Fine Command
- Acceleration Limit
- Acceleration Reference
- Acceleration Trim
- Actuator Diameter
- Actuator Diameter Unit
- Actuator Lead
- Actuator Lead Unit
- Actuator Type
- Adaptive Tuning Configuration
- Adaptive Tuning Gain Scaling Factor
- Analog Input 1
- Analog Input 2
- Analog Output 1
- Analog Output 2
- Auto Sag Configuration
- Auto Sag Slip Increment
- Auto Sag Slip Time Limit
- Auto Sag Start
- Axis Safety Data A
- Axis Safety Data B
- Axis Safety Faults
- Axis Safety Faults - RA
- Axis Safety State
- Axis Safety Status
- Axis Safety Status - RA
- Backlash Compensation Window
- Brake Prove Ramp Time
- Brake Slip Tolerance
- Brake Test Torque
- Break Frequency
- Break Voltage
- Bus Regulator Capacity
- CIP APR Faults
- CIP APR Faults - RA
- CIP Axis Alarms
- CIP Axis Alarms - RA
- CIP Axis Exception Action
- CIP Axis Exception Action - RA
- CIP Axis Faults
- CIP Axis Faults - RA
- CIP Axis I/O Status
- CIP Axis I/O Status - RA
- CIP Axis State
- CIP Axis Status
- CIP Axis Status - RA
- CIP Initialization Faults
- CIP Initialization Faults- RA
- CIP Start Inhibits
- CIP Start Inhibits - RA
- Coasting Time Limit
- Commutation Offset
- Commutation Offset Compensation
- Commutation Polarity
- Commutation Self-Sensing Current
- Connection Loss Stopping Action
- Control Method
- Control Mode
- Converter Capacity
- Converter Output Current
- Converter Output Power
- Current Command
- Current Disturbance
- Current Error
- Current Feedback
- Current Limit Source
- Current Reference
- Current Vector Limit
- DC Bus Voltage
- DC Injection Brake Current
- DC Injection Brake Time
- Deceleration Limit
- Digital Inputs
- Digital Outputs
- Feedback 1 Accel Filter Bandwidth
- Feedback 1 Accel Filter Taps
- Feedback 1 Battery Absolute
- Feedback 1 Cycle Interpolation
- Feedback 1 Cycle Resolution
- Feedback 1 Data Code
- Feedback 1 Data Length
- Feedback 1 Length
- Feedback 1 Loss Action
- Feedback 1 Polarity
- Feedback 1 Resolver Cable Balance
- Feedback 1 Resolver Excitation Frequency
- Feedback 1 Resolver Excitation Voltage
- Feedback 1 Resolver Transformer Ratio
- Feedback 1 Serial Number
- Feedback 1 Startup Method
- Feedback 1 Turns
- Feedback 1 Type
- Feedback 1 Unit
- Feedback 1 Velocity Filter Bandwidth
- Feedback 1 Velocity Filter Taps
- Feedback 2 Accel Filter Bandwidth
- Feedback 2 Accel Filter Taps
- Feedback 2 Battery Absolute
- Feedback 2 Cycle Interpolation
- Feedback 2 Cycle Resolution
- Feedback 2 Data Code
- Feedback 2 Data Length
- Feedback 2 Length
- Feedback 2 Loss Action
- Feedback 2 Polarity
- Feedback 2 Resolver Cable Balance
- Feedback 2 Resolver Excitation Frequency
- Feedback 2 Resolver Excitation Voltage
- Feedback 2 Resolver Transformer Ratio
- Feedback 2 Serial Number
- Feedback 2 Startup Method
- Feedback 2 Turns
- Feedback 2 Type
- Feedback 2 Unit
- Feedback 2 Velocity Filter Bandwidth
- Feedback 2 Velocity Filter Taps
- Feedback Commutation Aligned
- Feedback Data Loss User Limit
- Feedback Mode
- Feedback Noise User Limit
- Feedback Signal Loss User Limit
- Feedback Unit Ratio
- Flux Braking Enable
- Flux Current Error
- Flux Current Feedback
- Flux Current Reference
- Flux Integral Time Constant
- Flux Loop Bandwidth
- Flux Up Control
- Flux Up Time
- Flying Start Enable
- Flying Start Method
- Frequency Control Method
- Friction Compensation Sliding
- Friction Compensation Static
- Friction Compensation Viscous
- Friction Compensation Window
- Guard Faults
- Guard Status
- Home Torque Threshold
- Home Torque Time
- Induction Motor Flux Current
- Induction Motor Magnetization Reactance
- Induction Motor Rated Frequency
- Induction Motor Rated Slip Speed
- Induction Motor Rotor Leakage Reactance
- Induction Motor Rotor Resistance
- Induction Motor Stator Leakage Reactance
- Induction Motor Stator Resistance
- Inverter Capacity
- Inverter Overload Action
- Inverter Thermal Overload User Limit
- Linear Motor Damping Coefficient
- Linear Motor Integral Limit Switch
- Linear Motor Mass
- Linear Motor Max Speed
- Linear Motor Pole Pitch
- Linear Motor Rated Speed
- Load Observer Acceleration Estimate
- Load Observer Bandwidth
- Load Observer Configuration
- Load Observer Feedback Gain
- Load Observer Integrator Bandwidth
- Load Observer Torque Estimate
- Load Type
- Local Control
- Maximum Frequency
- Maximum Voltage
- Mechanical Brake Control
- Mechanical Brake Engage Delay
- Mechanical Brake Release Delay
- Motion Polarity
- Motion Resolution
- Motion Scaling Configuration
- Motion Unit
- Motor Capacity
- Motor Catalog Number
- Motor Data Source
- Motor Device Code
- Motor Electrical Angle
- Motor Integral Thermal Switch
- Motor Max Winding Temperature
- Motor Overload Action
- Motor Overload Limit
- Motor Overspeed User Limit
- Motor Phase Loss Limit
- Motor Polarity
- Motor Rated Continuous Current
- Motor Rated Output Power
- Motor Rated Peak Current
- Motor Rated Voltage
- Motor Thermal Overload User Limit
- Motor Type
- Motor Unit
- Motor Winding To Ambient Capacitance
- Motor Winding To Ambient Resistance
- Operative Current Limit
- Output Current
- Output Frequency
- Output Power
- Output Voltage
- Overtorque Limit
- Overtorque Limit Time
- PM Motor Extended Speed Permissive
- PM Motor Flux Saturation
- PM Motor Force Constant
- PM Motor Inductance
- PM Motor Ld Flux Saturation
- PM Motor Ld Inductance
- PM Motor Linear Bus Overvoltage Speed
- PM Motor Linear Max Extended Speed
- PM Motor Linear Voltage Constant
- PM Motor Lq Flux Saturation
- PM Motor Lq Inductance
- PM Motor Rated Force
- PM Motor Rated Torque
- PM Motor Resistance
- PM Motor Rotary Bus Overvoltage Speed
- PM Motor Rotary Max Extended Speed
- PM Motor Rotary Voltage Constant
- PM Motor Torque Constant
- Position Error
- Position Error Tolerance
- Position Error Tolerance Time
- Position Feedback 1
- Position Feedback 2
- Position Fine Command
- Position Integrator Bandwidth
- Position Integrator Control
- Position Integrator Output
- Position Integrator Preload
- Position Lead Lag Filter Bandwidth
- Position Lead Lag Filter Gain
- Position Lock Tolerance
- Position Loop Bandwidth
- Position Loop Output
- Position Notch Filter Frequency
- Position Reference
- Position Trim
- Position Unwind
- Power Loss Action
- Power Loss Threshold
- Power Loss Time
- Proving Configuration
- Ramp Acceleration
- Ramp Deceleration
- Ramp Jerk Control
- Ramp Velocity - Negative
- Ramp Velocity - Positive
- Registration 1 Negative Edge Position
- Registration 1 Negative Edge Time
- Registration 1 Positive Edge Position
- Registration 1 Positive Edge Time
- Registration 2 Negative Edge Position
- Registration 2 Negative Edge Time
- Registration 2 Positive Edge Position
- Registration 2 Positive Edge Time
- Resistive Brake Contact Delay
- Rotary Motor Damping Coefficient
- Rotary Motor Fan Cooling Derating
- Rotary Motor Fan Cooling Speed
- Rotary Motor Inertia
- Rotary Motor Max Speed
- Rotary Motor Poles
- Rotary Motor Rated Speed
- Run Boost
- Safe Stopping Action
- Safe Stopping Action Source
- Safe Torque Off Action
- Safe Torque Off Action Source
- Shutdown Action
- Skip Speed 1
- Skip Speed 2
- Skip Speed 3
- Skip Speed Band
- SLAT Configuration
- SLAT Set Point
- SLAT Time Delay
- Slip Compensation
- Start Boost
- Stopping Action
- Stopping Time Limit
- Stopping Torque
- System Inertia
- Torque Integral Time Constant
- Torque Lead Lag Filter Bandwidth
- Torque Lead Lag Filter Gain
- Torque Limit - Negative
- Torque Limit - Positive
- Torque Loop Bandwidth
- Torque Low Pass Filter Bandwidth
- Torque Low Pass Filter Bandwidth Estimate
- Torque Notch Filter Frequency
- Torque Notch Filter Frequency Estimate
- Torque Notch Filter High Frequency Limit
- Torque Notch Filter Low Frequency Limit
- Torque Notch Filter Magnitude Estimate
- Torque Notch Filter Tuning Threshold
- Torque Prove Current
- Torque Rate Limit
- Torque Reference
- Torque Reference Filtered
- Torque Reference Limited
- Torque Threshold
- Torque Trim
- Transmission Ratio Input
- Transmission Ratio Output
- Travel Mode
- Undertorque Limit
- Undertorque Limit Time
- Velocity Droop
- Velocity Error
- Velocity Error Tolerance
- Velocity Error Tolerance Time
- Velocity Feedback
- Velocity Feedforward Command
- Velocity Feedforward Gain
- Velocity Fine Command
- Velocity Integrator Bandwidth
- Velocity Integrator Control
- Velocity Integrator Output
- Velocity Integrator Preload
- Velocity Limit - Negative
- Velocity Limit - Positive
- Velocity Limit Source
- Velocity Lock Tolerance
- Velocity Loop Bandwidth
- Velocity Loop Output
- Velocity Low Pass Filter Bandwidth
- Velocity Negative Feedforward Gain
- Velocity Reference
- Velocity Standstill Window
- Velocity Threshold
- Velocity Trim
- Vertical Load Control
- Zero Speed
- Zero Speed Time
Provide Feedback