Process Valve Statistics Object (PVLVS)

Process Valve Statistics Object (PVLVS)

This information applies to the CompactLogix 5380P and ControlLogix 5580P controllers.
The Process Valve Statistics Object (PVLVS) instruction monitors a two-state (open and close) valve and records statistics for stroke times and stroke counts to aid in planning maintenance or diagnosing valve and actuator problems. The PVLVS instruction is designed to work with the PVLV (solenoid, motor, and hand operated) valve instruction.
The PVLVS instruction records these statistics:
  • Amount of time in the current state (closed, opening, opened, closing, stopped/other)
  • Amount of time the valve was in each state the last time it was in that state (closed, opening, opened, closing, stopped/other)
  • Maximum amount of time spent in each state (closed, opening, opened, closing, and stopped/other); these are the highest values achieved by the previous statistics
  • Total amount of time spent in each state (closed, opening, opened, closing, stopped/other)
  • Moving average of the last 10 closing (close stroke) times
  • Moving average of the last 10 opening (open stroke) times
  • Number of completed open strokes (from closed to opened)
  • Number of completed close strokes (from opened to closed)
  • Number of incomplete open strokes (from closed to opening and back to closed)
  • Number of incomplete close strokes (from opened to closing and back to opened)
  • Number of times the valve was in the stopped/other state
  • Number of open strokes that took longer than the configured Slow Open Time
  • Number of close strokes that took longer than the configured Slow Close Time
Available Languages
Ladder Diagram
PVLVS_ladder_availlang
Function Block Diagram
PVLVS_FBD_availlang
Structured Text
PVLVS (PVLVS_01);
Operands
IMPORTANT:
Unexpected operation may occur if:
  • Output tag operands are overwritten.
  • Members of a structure operand are overwritten.
  • Except when specified, structure operands are shared by multiple instructions.
There are data conversion rules for mixing numeric data types within an instruction. See Data conversions.
Configuration Operands
Operand
Type
Format
Description
PlantPAx Control
P_VALVE_STATISTICS
tag
Data structure required for proper operation of the instruction.
P_VALVE_STATISTICS Structure
Public members are standard, visible tag members that are programmatically accessible. Private, hidden members are used in HMI faceplates and are not programmatically accessible. Private members are listed in separate tables after public members.
Public Input Members
Data Type
Description
EnableIn
BOOL
Enable Input - System Defined Parameter
Default is true.
Inp_InitializeReq
BOOL
1 = Request to initialize the instruction. The instruction is normally initialized in instruction first run. Use this request when reinitialization is needed. The instruction clears this operand automatically.
Inp_Closed
BOOL
1 = Device is confirmed Closed.
Default is false.
Inp_Opened
BOOL
1 = Device is confirmed Opened.
Default is false.
Inp_StopOther
BOOL
1 = Device is confirmed Stopped / Other.
Default is false.
Cfg_HasStopOther
BOOL
1 = Device has Stopped or other state(s) to be monitored.
Default is false.
Cfg_SlowOpenTime
REAL
Maximum time Opening (seconds) before raising Sts_SlowOpen. Valid = 0.0 to 2147483.0 seconds.
Default is 10.0.
Cfg_SlowCloseTime
REAL
Maximum time Closing (seconds) before raising Sts_SlowClose. Valid = 0.0 to 2147483.0 seconds.
Default is 10.0.
PCmd_ClearTotTimes
BOOL
Program command to clear total time statistics.
Default is false.
PCmd_ClearMaxTimes
BOOL
Program command to clear maximum time statistics.
Default is false.
PCmd_ClearStrokeCounts
BOOL
Program command to clear stroke count statistics.
Default is false.
PCmd_ClearSlowCounts
BOOL
Program command to clear device slow count statistics.
Default is false.
PCmd_ClearMAvgs
BOOL
Program command to clear moving average stroke times.
Default is false.
Public Output Members
Data Type
Description
EnableOut
BOOL
Enable Output - System Defined Parameter
Val_CurrClosedTime
REAL
Current time in Closed state (seconds).
Val_LastClosedTime
REAL
Time in Closed state (seconds) last time device was closed.
Val_TotClosedTime
REAL
Accumulated time in Closed state (hours).
Val_MaxClosedTime
REAL
Maximum time in Closed state (hours) of any occurrence.
Val_CurrOpeningTime
REAL
Current time in Opening state (seconds).
Val_LastOpeningTime
REAL
Time in Opening state (seconds) last time device was opening.
Val_TotOpeningTime
REAL
Accumulated time in Opening state (hours).
Val_MaxOpeningTime
REAL
Maximum time in Opening state (hours) of any occurrence.
Val_MAvgOpeningTime
REAL
Moving average Open stroke time, last 10 complete open strokes (seconds).
Val_CurrOpenedTime
REAL
Current time in Opened state (seconds).
Val_LastOpenedTime
REAL
Time in Opened state (seconds) last time device was opened.
Val_TotOpenedTime
REAL
Accumulated time in Opened state (hours).
Val_MaxOpenedTime
REAL
Maximum time in Opened state (hours) of any occurrence.
Val_CurrClosingTime
REAL
Current time in Closing state (seconds).
Val_LastClosingTime
REAL
Time in Closing state (seconds) last time device was closing.
Val_TotClosingTime
REAL
Accumulated time in Closing state (hours).
Val_MaxClosingTime
REAL
Maximum time in Closing state (hours) of any occurrence.
Val_MAvgClosingTime
REAL
Maximum time in Closing state (seconds) of any occurrence.
Val_CurrStopOtherTime
REAL
Current time in Stopped / Other state (seconds).
Val_LastStopOtherTime
REAL
Time in Stopped / Other state (seconds) last time device was stopped (or other).
Val_TotStopOtherTime
REAL
Accumulated time in Stopped / Other state (hours).
Val_MaxStopOtherTime
REAL
Maximum time in Stopped / Other state (hours) of any occurrence.
Val_CpltOpenCount
DINT
Count of complete device Open strokes (Closed to Opened).
Val_CpltCloseCount
DINT
Count of complete device Close strokes (Opened to Closed).
Val_IncpltOpenCount
DINT
Count of incomplete device Open strokes (Closed - Moving - Closed).
Val_IncpltCloseCount
DINT
Count of incomplete device Close strokes (Opened - Moving - Opened).
Val_StopOtherCount
DINT
Count of device Stopped / Other occurrences.
Val_SlowOpenCount
DINT
Count of device Slow to Open occurrences.
Val_SlowCloseCount
DINT
Count of device Slow to Close occurrences.
Sts_SlowOpen
BOOL
1 = Last Closed to Opened stroke exceeded configured time threshold.
Sts_SlowClose
BOOL
1 = Last Opened to Closed stroke exceeded configured time threshold.
Sts_Err
BOOL
1 = Configuration Error: invalid Slow Open Time or Slow Close Time.
Sts_ErrSlowCloseTime
BOOL
1 = Error in configuration: Invalid SlowCloseTime timer preset (use 0.0 to 2147483.0).
Sts_ErrSlowOpenTime
BOOL
1 = Error in configuration: Invalid SlowOpenTime timer preset (use 0.0 to 2147483.0).
Private Input Members
Data Type
Description
MCmd_ClearMAvgs
BOOL
Maintenance command to clear moving average stroke times.
Default is false.
MCmd_ClearMaxTimes
BOOL
Maintenance command to clear maximum time statistics.
Default is false.
MCmd_ClearSlowCounts
BOOL
Maintenance command to clear device slow count statistics.
Default is false.
MCmd_ClearStrokeCounts
BOOL
Maintenance command to clear stroke count statistics.
Default is false.
MCmd_ClearTotTimes
BOOL
Maintenance command to clear total time statistics.
Default is false.
Operation
These diagrams illustrate the functionality of the PVLVS instruction:
PVLVSOperation_Inp_Closed
PVLVSOperation_Inp_Opening
PVLVSOperation_Inp_Opened
PVLVSOperation_Inp_Closing
PVLVSOperation_Inp_StopOther
PVLVSOperation_Inp_StopOtherCount
PVLVSOperation_IncpltOpenCount
PVLVSOperation_CpltOpenCount
PVLVSOperation_CpltCloseCount
PVLVSOperation_IncpltCloseCount
Configuration of Strings for HMI
Configure strings for HMI faceplates (FT View) and for the Logix Designer configuration dialog box. The strings are set to extended properties of tag items. Configure the strings in
Logix Designer
only.
  • Valve is confirmed Stopped / Other (in Logix Designer dialog box) – Description of Inp_StopOther item.
  • Description
  • Label for graphic symbol
  • Display Library for HMI Faceplate call-up
  • Instruction name
  • Area name
  • URL link
Monitor the PVLVS instruction
Use the operator faceplate from the PlantPAx library of Process objects for monitoring.
Affects Math Status Flags
No.
Major/Minor Faults
None specific to this instruction. See Index Through Arrays for array-indexing faults.
Execution
Ladder Diagram
Condition/State
Action Taken
Prescan
Rung-condition-out is cleared to false.
Total times, stroke counts and slow counts are maintained through a power cycle. Current times are cleared.
The internal state is set to
unknown
. When an input shows the valve in a known condition, the main logic transitions to the corresponding state.
Instruction first run
All commands that are automatically cleared each execution are cleared and ignored.
The instruction executes normally.
Rung-condition-in is false
Set rung-condition-out to rung-condition-in.
If this instruction is on a false rung, or if EnableIn is false in FBD, Total times, stroke counts, and slow counts are maintained, but Current times are cleared.
The internal state is set to
unknown
.
Copies the current time of the previous state to its last time and resets the current time (and accumulated 10ths of hours, if applicable).
The internal state is set to
unknown
(disabled).
When normal execution (Logic routine) is resumed, when an input shows the valve in a known condition, a transition to the corresponding state occurs.
Should scan all the retentive timers FALSE to stop them.
Rung-condition-in is true
Set rung-condition-out to rung-condition-in.
The instruction executes.
Postscan
Rung-condition-out is cleared to false.
Function Block Diagram
Condition/State
Action Taken
Prescan
See Prescan in the Ladder Diagram table.
Instruction first run
See Instruction first run in the Ladder Diagram table.
Instruction first scan
See Instruction first run in the Ladder Diagram table.
EnableIn is false
See Rung-condition-in is false in the Ladder Diagram table.
EnableIn is true
See Rung-condition-in is true in the Ladder Diagram table.
Postscan
EnableIn and EnableOut bits are cleared to false.
Structured Text
In Structured Text, EnableIn is always true during normal scan. Therefore, if the instruction is in the control path activated by the logic it will execute.
Condition/State
Action Taken
Prescan
See Prescan in the Ladder Diagram table.
Instruction first run
See Instruction first run in the Ladder Diagram table.
EnableIn is true
See Rung-condition-in is true in the Ladder Diagram table.
Postscan
EnableIn and EnableOut bits are cleared to false.
Example
This section shows how the PVLVS instruction collects statistics on a motor-operated valve. In this example, the motor-operated valve is controlled by using the PVLVS instruction. By naming the PVLVS instance tag the same as the PVLV tag plus ValveStats, the PVLVS instance tag is automatically linked at the HMI to the valve instance. In this example, the motor-operated valve is opened, closed, or the motor could stop moving while in travel before reaching either position. Statistics for all of these three states can be tracked by using the PVLVS instruction. In this example, the parameters Inp_Closed, Inp_Opened, and Inp_StopOther are connected to the parameters Sts_Closed, Sts_Opened, and Sts_Stopped of the PVLV instruction. The PVLVS instruction keeps track of completed strokes, plus open and close strokes that are slower than expected. The parameters Cfg_SlowOpenTime and Cfg_SlowCloseTime are set to 10, to indicate that any transition longer than 10 seconds is considered slow.
Ladder Diagram
PVLVS_ladder_example
Function Block Diagram
PVLVS_FBD_example
Structured Text
PVLVMO_ValveStat.Inp_Closed := PVLVMO.Sts_Closed;
PVLVMO_ValveStat.Inp_Opened := PVLVMO.Sts_Opened;
PVLVMO_ValveStat.Inp_StopOther := PVLVMO.Sts_Stopped;
PVLVS (PVLVMO_ValveStat);
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal