Reset SFC (SFR)

Reset SFC (SFR)

This information applies to the
CompactLogix
5370,
ControlLogix
5570,
Compact GuardLogix
5370,
GuardLogix
5570,
Compact GuardLogix
5380,
CompactLogix
5380,
CompactLogix
5480,
ControlLogix
5580, and
GuardLogix
5580 controllers.
The SFR instruction resets the execution of an SFC routine at a specified step.
Available Languages
Ladder Diagram
SFR_LD_avail_v31
Function Block
This instruction is not available in function block.
Structured Text
SFR(SFCRoutineName,StepName);
Operands
Ladder Diagram
Operand
Type
Format
Description
SFCRoutineName
ROUTINE
name
SFC routine to reset
StepName
SFC_STEP
tag
Target step where to resume execution
Structured Text
Operand
Type
Format
Description
SFCRoutineName
ROUTINE
name
SFC routine to reset
StepName
SFC_STEP
tag
Target step where to resume execution
See Structured Text Syntax for more information on the syntax of expressions within structured text.
Description
When the SFR instruction is enabled:
  • In the specified SFC routine, all stored actions stop executing (reset).
  • The SFC begins executing at the specified step.
  • If the target step is 0, the chart will be reset to is initial step.
The Logix implementation of the SFR instruction differs from that in the
PLC-5
controller. In the
PLC-5
controller, the SFR executes when the rung condition is true. After reset, the SFC would remain paused until the rung containing the SFR became false. This allowed the execution following a reset to be delayed. This pause/un-pause feature of the
PLC-5
SFR instruction was decoupled from the rung condition and moved into the SFP instruction.
Affects Math Status Flags
No
Fault Conditions
A major fault will occur if:
Fault Type
Fault Code
The routine type is not an SFC routine
4
85
Specified target step does not exist in the SFC routine
4
89
See Common Attributes for operand-related faults.
Execution
Ladder Diagram
Condition/State
Action Taken
Prescan
N/A
Rung-condition-inis false
N/A
Rung-condition-in is true
The instruction reset the specified SFC routine execution to a particular step.
Postscan
N/A
Structured Text
Condition/State
Action Taken
Prescan
N/A
Normal execution
The instruction reset the specified SFC routine execution to a particular step.
Postscan
N/A
Example
Ladder Diagram
SFR_LD_ex_v31
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal