Selected Summer (SSUM)
This information applies to the
CompactLogix
5370, ControlLogix
5570, Compact GuardLogix
5370, GuardLogix
5570, Compact GuardLogix
5380, CompactLogix
5380, CompactLogix
5480, ControlLogix
5580, and GuardLogix
5580 controllers.The Selected Summer (SSUM) instruction uses Boolean inputs to select real inputs to be algebraically summed.
Available Languages
Ladder Diagram
This instruction is not available in ladder diagram logic.
Function Block

Structured Text
SSUM(SSUM_tag);
Operands
Function Block
Operand | Type | Format | Description |
SSUM tag | SELECTED_SUMMER | Structure | SSUM structure |
SELECTABLE_SUMMER Structure
Input Parameter | Data Type | Description |
EnableIn | BOOL | Enable input. If false, the instruction does not execute and outputs are not updated.
Default is true. |
In1 | REAL | The first input to be summed.
Valid = any float
Default = 0.0 |
Gain1 | REAL | Gain for the first input.
Valid = any float
Default = 1.0 |
Select1 | BOOL | Selector signal for the first input.
Default is false. |
In2 | REAL | The second input to be summed.
Valid = any float
Default = 0.0 |
Gain2 | REAL | Gain for the second input.
Valid = any float
Default = 1.0 |
Select2 | BOOL | Selector signal for the second input.
Default is false. |
In3 | REAL | The third input to be summed.
Valid = any float
Default = 0.0 |
Gain3 | REAL | Gain for the third input.
Valid = any float
Default = 1.0 |
Select3 | BOOL | Selector signal for the third input.
Default is false. |
In4 | REAL | The fourth input to be summed.
Valid = any float
Default = 0.0 |
Gain4 | REAL | Gain for the fourth input.
Valid = any float
Default = 1.0 |
Select4 | BOOL | Selector signal for the fourth input.
Default is false. |
In5 | REAL | The fifth input to be summed.
Valid = any float
Default = 0.0 |
Gain5 | REAL | Gain for the fifth input.
Valid = any float
Default = 1.0 |
Select5 | BOOL | Selector signal for the fifth input.
Default is false. |
In6 | REAL | The sixth input to be summed.
Valid = any float
Default = 0.0 |
Gain6 | REAL | Gain for the sixth input.
Valid = any float
Default = 1.0 |
Select6 | BOOL | Selector signal for the sixth input.
Default is false. |
In7 | REAL | The seventh input to be summed.
Valid = any float
Default = 0.0 |
Gain7 | REAL | Gain for the seventh input.
Valid = any float
Default = 1.0 |
Select7 | BOOL | Selector signal for the seventh input.
Default is false. |
In8 | REAL | The eighth input to be summed.
Valid = any float
Default = 0.0 |
Gain8 | REAL | Gain for the eighth input.
Valid = any float
Default = 1.0 |
Select8 | BOOL | Selector signal for the eighth input.
Default is false. |
Bias | REAL | Bias signal input. The instruction adds the Bias to the sum of the inputs.
Valid = any float
Default = 0.0 |
Output Parameter | Data Type | Description |
EnableOut | BOOL | Indicates if instruction is enabled. Cleared to false if Out overflows. |
Out | REAL | The calculated output of the algorithm. |
Structured Text
Operand | Type | Format | Description |
SSUM tag | SELECTED_SUMMER | Structure | SSUM structure |
See Structured Text Syntax for more information on the syntax of expressions within structured text.
Description
The SSUM instruction operates as follows:
Condition | Action |
No In is selected | Out = Bias |
One or more In are selected | For all n where Selectn is true Out = ∑ (In n x Gainn ) + Bias |
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See Common Attributes for operand-related faults.
Execution
Function Block
Condition/State | Action Taken |
Prescan | EnableIn and EnableOut bits are cleared to false. |
Tag.EnableIn is false | EnableIn and EnableOut bits are cleared to false. |
Tag.EnableIn is true | EnableIn and EnableOut bits are set to true. The instruction executes. |
Instruction first run | N/A |
Instruction first scan | N/A |
Postscan | EnableIn and EnableOut bits are cleared to false. |
Structured Text
Condition/State | Action Taken |
Prescan | See Prescan in the Function Block table. |
Normal Execution | See Tag.EnableIn is true in the Function Block table. |
Postscan | See Postscan in the Function Block table. |
Example
The values of select1 and select 2 determine whether to select analog_input1 and analog_input2, respectively. The instruction then adds the selected inputs and places the result in Out.
Function Block

Structured Text
SSUM_01.In1 := analog_input1;
SSUM_01.Select1 := select1;
SSUM_01.In2 := analog_input2;
SSUM_01.Select2 := select2;
SSUM(SSUM_01);
selected_add := SSUM_01.Out;
Provide Feedback