Select Branch Diverge

The selection diverge branch represents two or more alternate paths of execution.
In a selection branch, only one alternate path is executed depending on which transition condition is true.
Available Languages
Ladder Diagram
Not Available
Function Block
Not Available
Sequential Function Chart
selectbranchdiverge1
Structured Text
Not Available
Description
A selected branch represents a choice between one step or group of steps or another step or group of steps (that is, an OR structure).
  • Only one branch executes.
  • By default the controller checks the transitions from left to right.
    • The controller takes the first true branch.
    • The
      Logix Designer
      application lets you change the order in which the controller checks the transitions.
selectbranchdivergebig
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.