Invalid Host Name

Invalid Host Name

The Host Name can have the following format:
a.b.c.d
a.b.c
a.b
a
where a, b, c, and d may contain only letters, digits, and hyphens. The total number of characters, including the ".", must be 48 or less.
The portions of a Host Name may be all numeric, except for the last portion. For example, you may have the following:
odin.cle.ab.com
123.cle.ab.com
123.123.123.com
123.123.com
but
NOT
:
123.123.123.123 (illegal)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal